Part Number: TMS320F28069M
Hi experts,
My customer is using the lab10 project for the original board.
RS calibration cannot be used because the customer's application requires a fast system startup. This may cause a sudden increase in speed due to the position of the rotor at startup. When the speed rises rapidly, the current also rises rapidly to USER_MOTOR_MAX_CURRENT.Is it possible to set this current rise lower than USER_MOTOR_MAX_CURRENT?
The customer wants to suppress the inrush current at startup.
Best regards,
Sasaki