Part Number: TMS320F28033

hello:
There is a register INTOSCnTRIM for internal clock calibration. The range of FINETRIM is -31 to 31. Is the value from -31 to 31 directly added to 10M?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28033

hello:
There is a register INTOSCnTRIM for internal clock calibration. The range of FINETRIM is -31 to 31. Is the value from -31 to 31 directly added to 10M?
Xiaolin,
This is correct, any change in the fine trim will move the internal 0 pin oscillator according to the DS TYP which is ~14kHz for each step.
Please keep in mind that this is signed magnitude format and not 2's complement so any register view in CCS will not show the negative value correctly.
FINETRIM register is used by the oscillator temperature compensation function to re-center the frequency based on measurement by the temp sensor.
Note that each device is trimmed from the factory to be ideally 10MHz at 30degC, so the value after device_cal function of both coarse and fine trim will be non-zero. It should be possible to realize ~10MHz across the temp range of the device by only modulating FINETRIM only.
Best,
Matthew