This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: FLASH write

Part Number: TMS320F28388D


Hi 

I am using F28388D controller,

I am basically try to load the Motorola S2 record format into the flash memory, the only thing i see in this flash is we can write max 128 bits at a time (16 bytes), but my s2 record is only 15 bytes so 1 byte will be left over.

i noticed there is a tool serial flash loader, do we have the source code for this tool available so that i can compare how are the bytes handled here so that i can use the feed back mechanism to handle to refresh ext WD.

thanks,

Nagesh