Part Number: TMS320F28388D
Hi,
I want to known what different the FIFO is between MCAN and SPI periphere?
Best
Jammy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Hi,
I want to known what different the FIFO is between MCAN and SPI periphere?
Best
Jammy
Jammy,
This is a very open-ended question. SPI and MCAN are very different peripherals, with no similarities whatsoever (perhaps with the exception that they are both serial peripherals). The application scenarios where they need to be used are also very different. In light of this, it would be meaningless to compare the FIFO of these 2 peripherals.
Hi Hareesh,
I want to known if i configure SPI RX FIFO with level 16,when recevived 16 datas from FIFO 0 to FIFO15,then I read out 8 datas from FIFO0 to FIFO7 , remain unread from FIFO8 to FIFO15,at that point,SPI recevied 8 datas,Do the 8 datas recevied occupy the place from FIFO 0-7 or the place from FIFO 8-15?
Jammy,
You don't have access to TXFIFO registers to directly write (or) RXFIFO registers to directly read. Any write to SPITXBUF register will write to TXFIFO and any read to SPIRXBUF register will read from RXFIFO.
Suppose RXFIFO is filled and users reads only 8 words then he would have read out contents of FIFO0-7 and the contents in FIFO8-15 gets moved to FIFO0-7. Subsequent data received will be filled from FIFO8 to FIFO15.
Regards,
Manoj