Hi Team,
I am using Urat for communication testing. I can communicate with the host PC (using USB port). I can see data transmission on RXD and TXD (using oscilloscope). I want to know why it is in GPIO28/29. (J5 43/44) Can't see any data transmission? Is it because I use USB for SCI communication, so I can only see data in RXD and TXD? Do I need to transmit data on GPIO28/29 to see the data transmission with an oscilloscope?
Thanks
Jenson