Hello,
I've been struggling with the docs regarding DCM MATH module. Version v13.1 is still available (and recommended) for advanced users. I consider myself an advanced user, so the plan was to use this library instead of the C2000Ware. However, the documentation seems to contain some misleading info.
For example:
- structure of PARK module type contains Sine and Cosine components (page 63 of the PDF), while the example indicates usage of Angle (page 64)
- SVGEN module is referenced via aci_se.h, while one would expect it to be svgen.h
Could you please advise which path should I proceed? Is the C2000Ware lib suitable for customized ACIM motor control?
Thank you,
Best regards,
Matej