Other Parts Discussed in Thread: TMS320F280025C, C2000WARE-MOTORCONTROL-SDK
Question1
I am looking for a low price microcontroller that support FOC mode for a BLDC Motor driver
BLDC Motor Specifications are as below
Battery Voltage = 72V
Control Mode = Field Oriented Control
Output Power =5.5KW
Peak Power = 8KW
Output Frequency Range =0- 600Hz
Question2 .What is the microcontroller frequency I have to consider to drive this motor. Is 60Hz frequency controller is enough ?