Other Parts Discussed in Thread: C2000WARE
Dear expert:
I am using TMS320F280025,I want to change the boot pins from GPIO24 and GPIO32 to AIO pins.I have read the chapter:"Configuring Boot Mode Pins" in the technical reference.However,I don't know how to modify the code to change the boot mode pins.At the same time,it seemed that I need to program the boot rom to modify the boot mode pins but not flash area.So I don't know where to modify the register's value by using XDS110.And also I think it is not by changing the application code to Configure Boot Mode Pins.Could you tell me the detailed operation steps to Configure Boot Mode Pins:
1.Where to modify the BMSP register's value?
2.Using which tool to program the BOOT ROM?
3.the detailed steps of the whole process.
4.After I modify the boot mode pins,I think the application code can not run only if I set the new boot mode pins to the right level,is that right?