Part Number: TMS320F28388D
Hi,
we're planning to use the F28388D in one of our next electronics designs. This upcoming design has lots of digital inputs coming from open collector circuits with pull-ups & RC-filtering and thus typically have quite slow rise and fall times in the range of a few 10µs.
I have already checked the F28388D's datasheet regarding potential limitations on transition rates (as is the case for the good old SN74HC CMOS logic family for example) - but couldn't find any. On the contrary - I was pleasantly surprised that all GPIOs seem to have a 150mV input hysteresis, as stated in datasheet section 7.6 - so I assume oscillations are not an issue.
Now, we wan't to be sure that we do not run into potential problems here, so my question is if there are any known issues regarding the F28388D's GPIO input structure in combination with slow input signals that might lead to an undesired device behavior or even damage the device (e.g. due to high shoot-trough currents in the GPIO's input buffer).
I want to point out that my question is not related to any communication, memory interfaces or similar where timing is essential of course. This is rather about "uncritical" input signals (e.g. momentary switches).
Appreciate your feedback. Thanks.
Best regards,
Sebastian