Other Parts Discussed in Thread: C2000WARE
Hi,
1). How to use PMBCTRL.FAST_MODE bit? If I want to below 100KHz, must I reset PMBCTRL.FAST_MODE = 0? And meanwhile shall I cooperate with the following registers?
* PMBTIMCLK
* PMBTIMSTSETUP
* PMBTIMBIDLE
* PMBTIMLOWTIMOUT
* PMBTIMHIGHTIMOUT
2). How to use PMBCTRL.SCL_DIR bit? If I want to Master, will I set SCL_DIR? Or if I want to slave, will I reset SCL_DIR?
3). How to use PMBCTRL.SCL_VALUE bit? Will I configure GPIO register to GPIO mode? And is the pin output mode or input mode?
4).How to use PMBCTRL.SCL_MODE bit? If I want to use PMBus, will I reset SCL_MODE=0 ? If I set SCL_MODE=1, how can it execute "PMBus clock pin configured as GPIO" ?
5).If I set PMBCTRL.I2CMODE=1, what functions of I2C can be used?