Other Parts Discussed in Thread: C2000WARE
Dear TI Team
as a part of initial evaluation of F28388D microcontroller we would like to perform some tests related to CAN support. What would be the most convenient way to demonstrate its full functionality:
CAN-A loopback test, PTP (CAN-A CAN-B) link test or there are some other tests already available? It would be highly appreciated if someone could share a sample code for these tests (to speed up the evaluation process).
Is there a possibility to employ internal hardware supported encryption for CAN traffic, or that feature only supports ethernet interface?
Thanks in advance
Best regards
Nenad Težak
P.S. Control cards for TMS320F28388D microcontrollers in combination with corresponding experimenter kits docking station are used