This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280025C: SP pointing out of stack after reset

Part Number: LAUNCHXL-F280025C
Other Parts Discussed in Thread: C2000WARE

HEllo Team, 

So , after the reset , i have my Code before Code start , when i reset and come to the start of my Code the SP Point to address :

which is actually out of stack.

stack is from 0x400 till 0x7f8.Could you please help me how to do correct this such that the SP Points to 0x400 ?

The second Problem is  After the Code it went to Code start  then started implementing 

stack pointer  init 

System pre_init 

after that i get this folloing error

Thanks

Ushma