Other Parts Discussed in Thread: TMS320F28027
Hi all !
I am working with TMS320F28027 . I have detected a strange behaviour on GPIO2, GPIO3, GPIO4, GPIO5 at conecting to my target. I use this outputs for alternative functions ePWM2A, ePWM2B ePWM3A, ePWM3B respectively. Them pull up function is disabled by default (see page 95 System control and reset). But when I connect to my target via XDS100 emulator, I see PWM impulses on this outputs, frequency of this impulses is 60 kHz. I used this value for setting my ePWM2 and ePWM3 in my code. It seems to start execute code and GPIOs behave as they are commanded by my code. But I have not run my code in debugger.
How do I solve this problem? Thanks in advance!