This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Lab01 project blinking Led issue

Part Number: LAUNCHXL-F28069M


Hello,

I have an issue with lab01 from instaspin_labs instruction. I have done everything with the instruction, but diode didn't want to blink. Value of variable "gMotorVars.UserErrorCode" is USER_Error_Code_NoError so it should be fine but it isn't. When i debbug lab01 project the diode turn off and then when i click Real-Time Silicon Mode and resume debugging the diode turns red permanently without blinking.

Please help i cannot solve this issue for weeks.