Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello,
I am new to TI microcontroller and after having managed to create a project from scratch to run the SD card example on the IDDK R2.2.1 board with the Delfino TMS320F28379D controlCARD R1.3, there is an error that I could not resolve. When I try to command the program to access/read/write to the card, it always jump to the ILLEGAL_ISR (from wait_ready in mmc_F2837x.c).
Except for creating a new CCS project to include the source code, I did not change any line of the example code.
I have tried to format the SD card by FAT32 or exFAT using PC but it would not help. Below are some screenshot about the error and linked resource.
The example location is "C:\ti\c2000\C2000Ware_MotorControl_SDK_3_02_00_00\c2000ware\device_support\f2837xd\examples\cpu1\sd_card\cpu01"
Thanks and best regard!