This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: ISR register save with FPU, TMU (R4H to R7H, XAR3?)

Part Number: TMS320F28075

Hi,

we get an FPU overflow (PIE 12.7) interrupt and wonder where it might come from.

Is there an issue with register save? The generated code is

        cpu_timer0_isr():
01484e:   761B        ASP          
01484f:   FFF0        PUSH         RB
014850:   0005        PUSH         AR1H:AR0H
014851:   ABBD        MOVL         *SP++, XT
014852:   AABD        MOVL         *SP++, XAR2
014853:   A8BD        MOVL         *SP++, XAR4
014854:   A0BD        MOVL         *SP++, XAR5
014855:   C2BD        MOVL         *SP++, XAR6
014856:   C3BD        MOVL         *SP++, XAR7
014857:   E20000BD    MOV32        *SP++, STF
014859:   E20300BD    MOV32        *SP++, R0H
01485b:   E20301BD    MOV32        *SP++, R1H
01485d:   E20302BD    MOV32        *SP++, R2H
01485f:   E20303BD    MOV32        *SP++, R3H
014861:   E6300600    SETFLG       RNDF32=1,RNDF64=1
014863:   FF69        SPM          #0
014864:   2942        CLRC         OVM|PAGE0
014865:   5616        CLRC         AMODE

I know Table 3-4. Register Pairs Saved and SP Positions for Context Saves in SPRU430F.

What with R4H to R7H? Are they not used by the compiler?
What with XAR3? Any problems with TMU?

Any other reason?

Compiler flags are:

-v28 -ml -mt --cla_support=cla1 --tmu_support=tmu0 --vcu_support=vcu2 -O2 --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/include" --include_path="C:/workspace/firmware/duc/rtos/include" --include_path="C:/workspace/firmware/duc/test_rtos_f2837xs_launchpad" --include_path="C:/workspace/firmware/duc/device_support/f2837xs/headers/include" --include_path="C:/workspace/firmware/duc/device_support/f2837xs/common/include" --define=_LAUNCHXL_F28377S -g --diag_suppress=10063 --diag_warning=225 --issue_remarks --verbose_diagnostics --quiet -k

Thanks and regards,

Frank

  • Hi Frank,

    I dont see  --float_support=fpu32 in your compiler flags. Could that be the reason?

    -Shantanu

  • Hi Shantanu,

    I do not believe that this is the reason. I am sorry, I copied the compiler flags out of CCS while playing around with the --fpu32 and --tmu0 options. It seems that --tmu0 implies --fpu32 (I cannot switch off --fpu32 when --tmu0 is on, see screenshot, but in the flag list I copied from, --fpu32 disappears).

    Anyway, the code generated is the same in both cases (with saving R0H to R3H, etc.), and the my question regarding the other registers is still the same.

    Thanks & regards,

    Frank

  • Hi Frank,

    Yes you are right about the flags. The FPU overflow interrupt takes place in case of an LVF flag, which is only triggered by math operations. 

    XAR3 should ideally be saved during the context save and we need to investigate why that is. R4H to R7H are not generally saved. 

    But if the interrupt being generated is 12.7, you need to trace the STF register and identify the exact point at which the interrupt is being generated. Can you assembly step through the code and let me know the exact point at which the interrupt is being generated?

    -Shantanu

  • Hi Shantanu,

    thank you for your support. We'll try to reproduce the error, seems difficult to catch it.

    Do you have any news concerning the register saves meanwhile?

    Thanks & regards,

    Frank

  • Hi Frank,

    High priority interrupts use fast context saves, which leads to only essential registers being saved. This is probably why you're observing less number of registers being saved. Can you try making it a low priority interrupt and let me know what you observe?

    -Shantanu

  • Hi Shantanu,

    I don't know how to make it alow low priority interrupt, IMHO on the C28xx CPU there is only one level for the masked interrupts. Sure there are different levels of register save: If I use an assembler routine, I am myself responsible to save the registers that are not saved automatically (Table 3.4 in SPRU430F), and if the C-ISR does not call any other function, the compiler might decide not to save registers not used. But as soon as there is any funcition call in the ISR (as in my example), I think all the registers that the compiler might use have to be saved.

    Thanks & regards,

    Frank

  • Hi Shantanu,

    thanks for the interesting links. IMHO, the PIE / PIEIER things and priorities do not influence the CPU / FPU register save / restore.

    But I tried the #pragma INTERRUPT (cpu_timer0_isr, LPI | HPI), and indeed, the save / restore is different, details see below. FPU manual SPRUHS1B says that SAVE / RESTORE R0H to R7H to / from shadow registers, this is for high priority ISRs (HPI) that cannot be nested. Unfortunately, the #pragma does not prevent that the user programs nesting. OK, there is a warning in the compiler manual SPRU514P.

    But in our case we want nested ISRs, so the default setting LPI is the correct one (save FPU registers on stack).

    So, I am still wondering what with R4H to R7H and XAR3 (and TMU?). If the compiler never uses them, all is fine, and we have to search for other reasons. Otherwise, it's a miracle that so many programs run...

    Thanks & regards,

    Frank

    Here the disassemblies for high and low priority ISRs:

    HPI:

    013da6:   761B        ASP          
    013da7:   0005        PUSH         AR1H:AR0H
    013da8:   ABBD        MOVL         *SP++, XT
    013da9:   AABD        MOVL         *SP++, XAR2
    013daa:   A8BD        MOVL         *SP++, XAR4
    013dab:   A0BD        MOVL         *SP++, XAR5
    013dac:   C2BD        MOVL         *SP++, XAR6
    013dad:   C3BD        MOVL         *SP++, XAR7
    013dae:   FFF0        PUSH         RB
    013daf:   E6700600    SAVE         RNDF32=1,RNDF64=1
    013db1:   FF69        SPM          #0
    013db2:   2942        CLRC         OVM|PAGE0
    013db3:   5616        CLRC         AMODE
    013db4:   761F0030    MOVW         DP, #0x30

    ...

    013e7b:   E562        RESTORE      
    013e7c:   FFF1        POP          RB
    013e7d:   C5BE        MOVL         XAR7, *--SP
    013e7e:   C4BE        MOVL         XAR6, *--SP
    013e7f:   83BE        MOVL         XAR5, *--SP
    013e80:   8ABE        MOVL         XAR4, *--SP
    013e81:   86BE        MOVL         XAR2, *--SP
    013e82:   87BE        MOVL         XT, *--SP
    013e83:   0003        POP          AR1H:AR0H
    013e84:   7617        NASP         
    013e85:   7602        IRET        

    LPI:

    013da6:   761B        ASP          
    013da7:   FFF0        PUSH         RB
    013da8:   0005        PUSH         AR1H:AR0H
    013da9:   ABBD        MOVL         *SP++, XT
    013daa:   AABD        MOVL         *SP++, XAR2
    013dab:   A8BD        MOVL         *SP++, XAR4
    013dac:   A0BD        MOVL         *SP++, XAR5
    013dad:   C2BD        MOVL         *SP++, XAR6
    013dae:   C3BD        MOVL         *SP++, XAR7
    013daf:   E20000BD    MOV32        *SP++, STF
    013db1:   E20300BD    MOV32        *SP++, R0H
    013db3:   E20301BD    MOV32        *SP++, R1H
    013db5:   E20302BD    MOV32        *SP++, R2H
    013db7:   E20303BD    MOV32        *SP++, R3H
    013db9:   E6300600    SETFLG       RNDF32=1,RNDF64=1
    013dbb:   FF69        SPM          #0
    013dbc:   2942        CLRC         OVM|PAGE0
    013dbd:   5616        CLRC         AMODE
    013dbe:   761F0030    MOVW         DP, #0x30

    ...

    013e85:   E2AF03BE    MOV32        R3H, *--SP, UNCF
    013e87:   E2AF02BE    MOV32        R2H, *--SP, UNCF
    013e89:   E2AF01BE    MOV32        R1H, *--SP, UNCF
    013e8b:   E2AF00BE    MOV32        R0H, *--SP, UNCF
    013e8d:   E28000BE    MOV32        STF, *--SP
    013e8f:   C5BE        MOVL         XAR7, *--SP
    013e90:   C4BE        MOVL         XAR6, *--SP
    013e91:   83BE        MOVL         XAR5, *--SP
    013e92:   8ABE        MOVL         XAR4, *--SP
    013e93:   86BE        MOVL         XAR2, *--SP
    013e94:   87BE        MOVL         XT, *--SP
    013e95:   0003        POP          AR1H:AR0H
    013e96:   3B30        SETC         INTM|DBGM
    013e97:   FFF1        POP          RB
    013e98:   7617        NASP         
    013e99:   7602        IRET

  • Frank,

    I wonder if this is a function of the optimisation. Can you revert the optimisation levels to off and do not optimise for code size? If the compiler senses that the XAR3 is not being used, it may not save it. 

    -Shantanu

  • Shantanu,

    I think this cannot be a function of optmisation (-Ox flag), if there are function calls in the ISR. These functions may be compiled with different optimisation (e.g. in a library) the compiler actually does not know about.

    Thanks & regards,

    Frank