Hi expert,
My customer is using TMS320F28034 now. But there was an error of Error -1015 when downloading the code. The customer has already tested the wait BOOT mode by referring to the following link and picture 1. However, it shows that the connection is still unsuccessful, and the password value cannot be monitored, as shown in picture 2. The program cannot run after power-on. Could it be the internal damage of the chip?

picture 1

picture 2
Could you please kindly help me about this issue? Thanks a lot!
BR
Julia