Hi
I'm concerned about the hex file generation issue.
For example.
Below is the hex file's first 3 lines.
:020000040008F2
:040000000048351669
:20000400B2BDAABDA2BDE20304BDE20305BDE20306BDE20307BDFE12761F03248D40C9C0E7
I know that the Hex file is " ALIGN(4)", so the third line begins with 0x80004,not 0x80002 .
The data in 0x80003 and 0x80004 is neglected,because the default data is 0x0FFFF.
Is it possible for the HEX file to generate the default value together with 0x80003 and 0x80004.
I'd like to get hex file with a countinouse address file to be used in the bootloader application. .
Regards
Arrow