This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2xPM_Sensorless Failed in CW Closed Loop

The 2xPM_Sensorless project works great except the following problem.

In BUILD LEVEL6, when SpeedRef1 is set to negative value, and lsw1 = 1, the motor spins Clock Wise without problem; however, when lsw1 is set to 2, i.e., close the loop with the estimated angle smo1.Theta, the motor stalls, and CCSv4 gets out of control. To be clearer, CCW closed loop with the estimated angle works perfectly. Please advise.