Part Number: TMS320F280025C
Other Parts Discussed in Thread: LAUNCHXL-F280025C, SYSCONFIG
Hi,
I apologize for my level of English.
Firstly I work on the LAUNCHXL-F280025C to developp a digital regulation on electronic power solutions. I developed the PWM functions with the dutycycle ,phase settings etc...
And now after browsing the forum for several days I am stuck on CMPSS setiings. I want to trip CMPSS and shut down all EPWM (for protections OCP/ OVP etc...).
It work correctly when i use only two ADCIN : only with XBAR_MUX00 and XBAR_MUX02 but not with another.
Why ? Can you explain me please ?
I join my code.
#include <f28002x_device.h>
#include "driverlib.h"
#include "utils.h"
#include "device.h"
#include "board.h"
#include "config.h"
float init_EPWM();
void init_cmpss();
void main(void)
{
// Initialize device clock and peripherals
Device_init();
// Disable pin locks and enable internal pullups.
Device_initGPIO();
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
Interrupt_initModule();
// Initialize the PIE vector table with pointers to the shell Interrupt Service Routines (ISR).
Interrupt_initVectorTable();
// board.c and board.h generate by sysconfig
Board_init();
// Disable sync and clock to PWM
SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
// Configure COMP1H
init_cmpss(CMPSS1_BASE);
init_cmpss(CMPSS2_BASE);
// initEPWM1 - Configure ePWM1
float tbclk = init_EPWM(myEPWM1_BASE);
// initEPWM2 - Configure ePWM2
tbclk = init_EPWM(myEPWM2_BASE);
// Configure phase between PWM1 & PWM2. PWM1 is configure as master and ePWM2 as slaves.
EPWM_disablePhaseShiftLoad(myEPWM1_BASE);
EPWM_setPhaseShift(myEPWM1_BASE, 0U);
// ePWM1 SYNCO is generated on CTR=0
EPWM_enableSyncOutPulseSource(myEPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_CNTR_ZERO);
// Configure phase shift for EPWM2 & 3
set_phase(myEPWM2_BASE, PHI);
EPWM_setSyncInPulseSource(myEPWM2_BASE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
EPWM_enablePhaseShiftLoad(myEPWM2_BASE);
// Calculate delays
get_delays_FED_RED(myEPWM1_BASE, tbclk);
get_delays_FED_RED(myEPWM2_BASE, tbclk);
// Enable sync and clock to PWM
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
EINT;
ERTM;
while(1)
{
// Trip flag is set when CTRIP signal is asserted
if((EPWM_getTripZoneFlagStatus(myEPWM1_BASE) & EPWM_TZ_FLAG_OST) != 0U && (EPWM_getTripZoneFlagStatus(myEPWM2_BASE) & EPWM_TZ_FLAG_OST) != 0U)
{
// Wait for comparator CTRIP to de-assert
while((CMPSS_getStatus(CMPSS1_BASE) & CMPSS_STS_HI_FILTOUT) != 0U && (CMPSS_getStatus(CMPSS2_BASE) & CMPSS_STS_HI_FILTOUT) != 0U)
{
}
// Clear trip flags
EPWM_clearTripZoneFlag(myEPWM1_BASE, EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_OST);
EPWM_clearTripZoneFlag(myEPWM2_BASE, EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_OST);
}
}
}
float init_EPWM(base)
{
float PWM_TBPRD;
float PWM_CMPA;
EPWM_ClockDivider PWM_PARAM_PRESCALER;
EPWM_HSClockDivider PWM_PARAM_HIGHSPEEDPRESCALER;
float TBCLK;
get_pwm_clock_from_freq(&PWM_TBPRD , &PWM_CMPA , &PWM_PARAM_PRESCALER , &PWM_PARAM_HIGHSPEEDPRESCALER, &TBCLK);
// Parameters
EPWM_setTimeBasePeriod(base, (uint16_t)PWM_TBPRD);
EPWM_setCounterCompareValue(base, EPWM_COUNTER_COMPARE_A, (uint16_t)PWM_CMPA);
EPWM_setPhaseShift(base, 0U);
EPWM_setTimeBaseCounter(base, 0U);
EPWM_setTimeBaseCounterMode(base, EPWM_COUNTER_MODE_UP_DOWN);
EPWM_disablePhaseShiftLoad(base);
EPWM_setClockPrescaler(base, PWM_PARAM_PRESCALER, PWM_PARAM_HIGHSPEEDPRESCALER);
// Set up shadowing
EPWM_setCounterCompareShadowLoadMode(base, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO);
// Set actions
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
// Trip zone
// Configure ePWM1x to output low on TZx TRIP
EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);
EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_LOW);
// Trigger event when DCBH is high
EPWM_setTripZoneDigitalCompareEventCondition(base, EPWM_TZ_DC_OUTPUT_B1, EPWM_TZ_EVENT_DCXH_HIGH);
// Configure DCBH to use TRIP4 as an input
EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN4, EPWM_DC_TYPE_DCBH);
// Enable DCB as OST
EPWM_enableTripZoneSignals(base, EPWM_TZ_SIGNAL_DCBEVT1);
// Configure the DCB path to be unfiltered and asynchronous
EPWM_setDigitalCompareEventSource(base, EPWM_DC_MODULE_B, EPWM_DC_EVENT_1, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL);
// Configure TRIP4 to be CTRIP1H using the ePWM X-BAR
XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX00_CMPSS1_CTRIPH);
XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX02_CMPSS2_CTRIPH);
XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX06_CMPSS4_CTRIPH);
// See the ePWM X-BAR Mux configuration table
XBAR_enableEPWMMux(XBAR_TRIP4, XBAR_MUX00, XBAR_MUX02 | XBAR_MUX06 );
// Clear trip flags
EPWM_clearTripZoneFlag(base, EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_OST);
return TBCLK;
}
{
// Sets up the rising edge delay input signal.
EPWM_setFallingEdgeDeadBandDelayInput(base, EPWM_DB_INPUT_EPWMA);
// Sets up the falling edge delay input signal.
EPWM_setRisingEdgeDeadBandDelayInput(base, EPWM_DB_INPUT_EPWMA);
// This function sets the FED count value, this one should be less than 16384.
EPWM_setFallingEdgeDelayCount(base, DBFED);
// This function sets the RED count value, this one should be less than 16384.
EPWM_setRisingEdgeDelayCount(base, DBRED);
// This function sets up the polarity : EPWM_DB_POLARITY_ACTIVE_HIGH => polarity is not inverted and EPWM_DB_POLARITY_ACTIVE_LOW => polarity is inverted.
EPWM_setDeadBandDelayPolarity(base, EPWM_DB_RED, EPWM_DB_POLARITY_ACTIVE_HIGH);
EPWM_setDeadBandDelayPolarity(base, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_HIGH);
// This function sets up the dead band delay mode. The enableDelayMode determines if a dead band delay should be applied.
EPWM_setDeadBandDelayMode(base, EPWM_DB_RED, true);
EPWM_setDeadBandDelayMode(base, EPWM_DB_FED, true);
//EPWM_setDeadBandOutputSwapMode(myEPWM2_BASE, EPWM_DB_OUTPUT_A, false);
EPWM_setDeadBandOutputSwapMode(base, EPWM_DB_OUTPUT_B, false);
}
void set_delays(uint32_t base, uint16_t DBFED, uint16_t DBRED)
void init_cmpss(base)
{
// Enable CMPSS and configure the negative input signal to come from the DAC
CMPSS_enableModule(base);
CMPSS_configHighComparator(base, CMPSS_INSRC_DAC);
// Use VDDA as the reference for the DAC and set DAC value to midpoint for arbitrary reference.
CMPSS_configDAC(base, CMPSS_DACREF_VDDA | CMPSS_DACVAL_SYSCLK | CMPSS_DACSRC_SHDW);
CMPSS_setDACValueHigh(base, 1024);
// Configure the output signals. Both CTRIPH and CTRIPOUTH will be fed by the asynchronous comparator output.
CMPSS_configOutputsHigh(base, CMPSS_TRIP_ASYNC_COMP | CMPSS_TRIPOUT_ASYNC_COMP);
}