Hello,
Can I create a GUI Composer 2 stand alone program that downloads an .out file to the target without uploading .out file to the cloud?
Thanks,
Stephen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can I create a GUI Composer 2 stand alone program that downloads an .out file to the target without uploading .out file to the cloud?
Thanks,
Stephen
Hello Stephen,
I assume that the issue is with security where you do not which to upload the out file to a server - just to export to a standalone GC app that contains the out file. If that is the case, perhaps one workaround is to upload a dummy out of the same name and then after the solution is exported to a standalone app, you can replace the out file in the generated zip with the actual one?
ki