Part Number: DRV8301-69M-KIT
Hi TI,
We are using a motor of 2KW(48V) which can go up to 4000rpm. But when we set the speed ref to 2000rpm motor is not able to spin more than 1600rpm. We have increased the saturation limit of PI (speed and current) control from _IQ(0.5) to _IQ(0.9) but we couldn't reach the max rpm.
What is limiting the motor to reach the max rpm.
Thanks