Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi, I'm starting from the dual axis example and want to add core 2 with basic IPC. Not clear on the correct way to add this
All the dual core examples use the libraries starting with "F2837xD_xxxx", but the dual axis project uses the libraries from "c2000ware\driverlib\f2837xd\driverlib\...". There is an ipc.[ch] file here, so I assume this would be the correct one to use.
So would I just drag the ipc.c file from driverlib folder into my existing src_driver folder with the other driver source files? The IPC code is similar, but not exactly the same.
Also, if I'm correct about the above, are there any example using the driverlib code, they all seem to be the F2837xD code
thanks