Part Number: TMS320F28377S
Hi experts,
In the F28377 application, we need to use the EMIP1 function. It occupies the F28377 boot pin GPIO72. So we changed the GPIO72 boot function to GPIO142 (previously GPIO72 and GPIO84 boot, Now GPIO142 and GPIO84 boot). But after changing the boot pin, there is a certain probability that after the hardware reset or programing to flash, it will not boot. The status of GPIO72 is still relevant, please help analyze this issue, thank you!
Here is the register value(read from ccs):
Z1_BOOTCTRL Register:0x8F55FF5A
Z2_BOOTCTRL Register:0xFFFFFFFF