Part Number: TMS320F28377S
In the note below, the ADCINA3, ADCINB5, ADCINC5, ADCIND2 pins are used for simultaneous sampling.
Can I use a different pin than the example for simultaneous sampling?
ADCINA3, ADCINB5, ADCINC5, ADCIND2 fixed? Or is it possible to use other pins?
9.3.3 Achieving Simultaneous Sampling
While the Type 4 ADC does not have dual S+H circuits, it is easy to achieve simultaneous sampling.
This is accomplished by setting the SOC triggers on two or more ADC modules to use the same trigger source.
The example below demonstrates x4 simultaneous sampling based on an ePWM3 event. ADCINA3, ADCINB5, ADCINC5, and ADCIND2 are sampled.
~~~
please answer about my question.
thank you