We have tried with the new serial flash programmer tool.
It works as what was described in the demo if we follow it exactly.
(Single Bank LFU with Device Reset on F28002x User Guide)
In this demo, the application file is f28002x_lfu_singlebankBANK0FLASH.txt but for us, we have our own application txt file.
Is there any other additional steps we need to do if we want to program the MCU ?
We use hex2000.exe tool to convert the application.out to application.txt. Then, we rerun the command again but replacing the
f28002x_lfu_singlebankBANK0FLASH.txt to application.txt.
Below is the command we use :
serial_flash_programmer_appln.exe -d f28002x -k f28002x_sci_flash_kernel.txt -a application.txt -b 9600 -p COM8
Actual Result : The data transfer was halted, it stops after 46 06 00 90 7C 91 22 56 AC 28 18 00 are transferred.
Does anyone have any idea about what are the mistake we made ?