I used DATA_SECTION many times for applications for storing the data, but never had the need to initialize those variables.
I am storing long data of arrays in DATA_SECTION in XINTF zone 7.
If all the variables needs to be initialized with same values, i would use 'for loop'
If number of variables are small, i would initialize individually.
Below array is for example. Actual size of the buffer would be around 200+ length.
Eg: Array_Input_Buffer[] = {1, 1.11896985452742, 1.08979021355160,0.938253665384576};
how to initialize the buffer ?
I am using CCS9 with v20.2.4 LTS compiler.