This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-BUCKCONV: DC-DC Step up converter

Part Number: BOOSTXL-BUCKCONV


I am Engr. Syed Farhan Ali Naqvi a Research Assistant at Sejong University. I have contacted you regarding our ongoing research project in the lab. We are looking for a DC-DC Step-up/boost converter for a single PV Cell having an efficiency of more than 90% with specifications as follow:
Vin (startup+operation) = <400mV
Iin= 200~800mA
Vout= 5V
Iout= >20mA

I am looking forward to hearing from you.