Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: TMS320F28388D
Hello,
I'm trying to work with Simulink to program TMDSCNCD28388D.
I build some simple models like a LED blinking or a pulse on a GPIO.
I do Build, Deploy and Run with a model setting the hardware as F2838x-M4 and nothing happens.
Then I do the same with the hardware as F2838x-C28x using CPU1 (and different GPIOs) and both codes start executing.
When I remove the power supply and restart the program does not correcly boot from flash.
I followed the instruction on the "TMS320F28388D controlCARD Information Guide" setting the switch S2 to 1-1.
What could I be missing?
J. P.