This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: TMS320F28075 on C2000-GAGN burning chip PCBA can not be repeated burning.

Part Number: TMS320F28075
Other Parts Discussed in Thread: TMS320F28027, TMS320F28033, TMS320F28016

Hello!

There are eco changes to be rewritten

The TMS320F28075 on the C2000-GAGN burning chip PCBA can not be repeated.

This C2000-GAGN can be burned for the first time, but the reburning procedure is not acceptable. It can be burned only after being erased in the previous way, but it is impossible for me to cooperate with the oldest tools.

Since you bought this C2000-GAGN, you should be able to burn it and erase it, but it will prompt Executing Main Process when you burn it again.

ERROR 23: MCU device init.

Failed

At present, TMS320F28075 TMS320F28016 has this phenomenon. TMS320F28033 TMS320F28027 can be repeated.

1, chip processing is encrypted, but only 28075 and 28016 can not be repeated.

2, decryption process, in the CSM/DCSM security Passwords interface Defined Password, enter the corresponding password can be unlock device. If the password is incorrect, GO will prompt CSM unlock error.

Project urgent, please help to prioritize.

Very urgent, thank you!

8182.erase and program process in C2000-GANG (1).pptxerase and program process in CCS Uniflash.pptx