Other Parts Discussed in Thread: LAUNCHXL-F280049C
Hi E2E,
Our customer is using the Launchxl-f28049c launchpad to program a standalone MCU TMS320F28075. They're using the launchpad's onboard emulator XDS110 to program externally the TMS320F28075. They can verify the test connections successfully on Code composer studio, but when they debug the F2807x example code it gives the following error.
C28xx_CPU1: Error connecting to the target: (Error -1015 @ 0x0) Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
Your assistance to solve the error is appreciated.
Regards,
Carlo