Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE
Dear sir,
1. I am trying to communicate with external device using SPI(which is configured in the CM4) if i keep CM4 in debug all signals like MOSI,CLOCK,CHIP SELECT are not coming out from Chip(DSP) ,if i keep CM4 in full run i am able to see all signals coming properly what may be the issue??. I am using driver examples which have given by TI for SPI communication.
2. If i keep CM4 in debug it wont work as expected, even i tried toggling GPIO by keeping cm4 in debug the pin is not toggling but if i come out of the debug and make CM4 full run ,toggling is happening, what may be the issue? please help me to resolve this issue.
Thanks & Regards
Maheshwar P