Other Parts Discussed in Thread: C2000WARE
Hi all:
The demo code I used is "C2000_SDK\C2000Ware_1_00_03_00\device_support\f2833x\examples\mcbsp_loopback_dma".
The gpio setting here:
//GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 3; // GPIO12 is MDXB pin
GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 3; // GPIO24 is MDXB pin
//GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 3; // GPIO13 is MDRB pin
GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 3; // GPIO25 is MDRB pin
//GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 3; // GPIO14 is MCLKXB pin
GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 3; // GPIO26 is MCLKXB pin
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 3; // GPIO3 is MCLKRB pin
//GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 1; // GPIO60 is MCLKRB pin
//GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 3; // GPIO15 is MFSXB pin
GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 3; // GPIO27 is MFSXB pin
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 3; // GPIO1 is MFSRB pin
//GpioCtrlRegs.GPBMUX2.bit.GPIO61 = 1; // GPIO61 is MFSRB pin.
1. I am confused with the MFSXB and MFSRB. They are two pins and I think the function of these pins is "pin select" in spi protcol which "CS". Can I use just one pin as "CS"?
2. The CLK pin, it should be provided by SPI master but in Mcbsp, it has two clock, ans I find they can be internally connected in clock stop mode which means I can use one pin as CLK?
Thanks
Li