Part Number: TMS320F28388D
Hi,
when I debug the DSP, both "CPU reset" and "Restart" buttons are available and I can do both of them for the CPU1 and CPU2 as is shown in the following picture.

However, when I want to do the same thing for the CM core, there is no available "CPU reset" button. Also, the "Reset" button does not work. The following picture shows this problem.

Note: I also checked .gel files of CPU1 and CM and compared them with each other. I realized that there is no code in the "OnRestart ()" callback function of CM's .gel file. I thought this explanation might be relevant to my problem. The following picture is a part of CM's .gel file is related to its "CPU reset and "Restart".

And the following picture is a part of CM's .gel file is related to its "CPU reset and "Restart".

So, my question is that how can I do "restart" and "CPU reset" for the CM.
Best,
Alex