Part Number: SM320F28335-EP
Other Parts Discussed in Thread: TMS320F28335, UNIFLASH, TMDSCNCD28335
Hello,
I'm working with a self developed board with the SM320F28335-EP device,
Code Composer Studio : Version: 10.4.0.00006 and
Spectrum Digital XDS100V2 TI-14PIN JTAG Emulator.
Triyng at first time to debug some easy application (led blink example) I received allways the same error:

C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: Flash Programmer: Warning: The configured device (TMS320F28335), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: File Loader: Verification failed: Values at address 0x08081@Program do not match Please verify target memory and memory map.
C28xx: GEL: File: C:\Users\103011\workspace_v10\Example_2833xLEDBlink\Debug\Example_2833xLEDBlink.out: a data verification error occurred, file load failed.
After checking some forums and finding threads with similar issues, I fogot to use Code Composer and try to read directly the memory of the device with UniFlash (Version: 6.4.0.3394).
With UniFlash I can read the memory of the device. Because it seems to have a locked device, I have checked the register 0x33fff8 with the next results:

0x0000 in all registers.
I seems that the device is locked.
In the "Setting & Utilities" tab of UniFlash, I have try to unlock the device, then to test the Checksum, to change the password, to perfomr Frequency test and I became allwais the same error: