Part Number: TIDM-1000
Hi,
I was testing the TIDM-1000 for closed voltage and current loop, but can only achieved a power factor of 0.72. My AC input was 230V, 60Hz, Vbus output measured about 600Vdc. Vbus was connected to a dc-dc, step down to about 37Vdc and a 3 ohm load.
1. Like to check if is possible to improve the power factor?
2. Is it possible to increase the Vbus voltage?
Thank you.
Regards,
GK