Part Number: TMS320F28379D
Hello,
i have a problem starting CPU1. Compiling and linking is doing fine on both cores. Then when i start the debugging, the CPU1 is stuck in a do while loop.
The do while loop is in the c28xxhw.c file of the SPI_EtherCAT_slave_stack code:

the variable u16PdiCtrl is always 0xFFFF when it reads from the ESC and never leaves the loop.
Do you have any idea why this is or how can i debug this better?
If you need more informations please let me know.
Thank you for helping
Best regards