Hello everybody,
The three phase PFC controller program was developed in CCS 3.3 using control card F28035 RAM, now I want to flash it, the following changes I made to run it from flash.
Option – customize – debug properties – perform go main automatic – disable.
- connect to the target at the start – disable.
- program/project/CIO – load program after build – disable.
Selected F2803X_FLASH as option to run program.
After rebuilt all, following procedure is used to flash it.
TOOL – F28XX on-chip flash programmer – operation load [XX.out] file,
And then click on erase.program.verify – then click on RUN,
This above said procedure works with out any error, a code included in the ISR to toggle the port-34 works fine, but the instruction written using IQ maths library doesn’t work, as it works in RAM.
What changes are required to successful run from flash?
Thanks in advance.