Part Number: TMS320F28377D
On this chip, how can I determine if the chip is in sci bootloading mode. I have TRST = 0, GPIO72 = 0, GPIO84 = 1. Is there any feedback over GPIOs or LEDs? Or do I need to program F2837xD_sci_flash_kernels_cpu01 to set a GPIO high to determine the bootloading software is running?