Other Parts Discussed in Thread: CONTROLSUITE
Hi,
In HVMTRPFC kit,
1. what is the maximum current and voltage rating in rms?
2.what is the shape of the current?
3.If i want to run the motor continously, how long this kit can provide the rated output, continously?
4. what is max and min. output frequency i can achieve?
5.whether F28035 has space vector PWM option?
6.what are protection circuit available in this kit?
Thanks & Regards,
sheik