Part Number: TMS320F2812
Hi
Posting in behalf of customer (cannot post in E2E, due system error)
"We have a TMS320F2812 application that is exhibiting a problem with the UART when running standalone. Upon power up, the activity indicator LED blinks telling us that the software is executing and timer interrupts are occurring properly. In about 30% of the power turn on events the UART does not function, the DSP does not respond to serial communications. Asserting the reset pin without power cycling brings the UART back into operation. What is causing this issue and how do we get around it? "
Thank you in advance.
Regards,
Maynard