Part Number: TIEVM-HV-1PH-DCAC
Other Parts Discussed in Thread: TIDM-HV-1PH-DCAC
Hi experts,
Please let me check about TIDM-HV-1PH-DCAC.https://www.tij.co.jp/tool/jp/TIEVM-HV-1PH-DCAC
This reference design can be used to achieve the following
Switching frequency: 20kHz
Output: 110Vrms
Output frequency: 60 Hz
Using this reference design as a guide, can I modify the software of the C2000 to achieve the following?
Switching frequency: 100kHz
Output: 110Vrms
Output frequency: 30kHz
My concern is that I could not determine if the C2000 (F2837xD and F28004x) can support a switching frequency of 100kHz. Based on TIDUB21D's "2.2.2.6 F2837x and F2807x" and the C2000's PWM performance, I believe it can, but any advice would be appreciated. We will make changes to each component if necessary to achieve the specifications.
Best regards,
O.H