Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSCNCD28388D
We have a project using the TMDSCNCD28388D Control Card board. We keep having problems and have tracked it down to shorted VDD_3V3 and VDD_1V2 rails. The VDDA_3V3 is not shorted.
The only DIO we are currently using are 15 PWM output signals to drive Infineon 1EDC30I12MHXUMA1 gate driver ICs.
We have gone through 6 boards, and have not been able to figure out what the issue is.
I did notice some of the analog inputs max out around 3.8V, but I think the TPD4E001QDBVRQ1 on the DEV board would clamp them to 3.3V.
The Firmware engineer has noted the board has failed a few times (rails shorted) during or right after flashing. We are using the onboard programmer.