Part Number: TMS320F280049C
Other Parts Discussed in Thread: TMDSCNCD280049C
Hi,
I had a look at the compliance pattern in the bsd file (sprm690a) for boundary scan for the F280049C device.
There I can see the following:
attribute COMPLIANCE_PATTERNS of F28004x : entity is
"(XRSn)" &
"(0)";
Is this correct? I think XRSn should be "1" for boundary scan not "0" (?).
Thanks and best regards,
Patrick