Part Number: TMS320F28388D
Hello everyone,
I am working with the TMS320F28388D. I created a debug configuration with which I am able to flash all cores in the MCU (CPU1 / CPU2 / CM) and start debugging successfully.
To be able to debug running applications I would like to connect CCS to a running Application without reflashing everything.
I thought I could achieve this by changing the option of the launch configuration to only load symbols and not the program. Unfortunately, this isn't working. CCS is connecting to every core, but the application stops working after the connect and only a power cycle helps. But the power cycle will cause CCS to lose connection.
What do I need to do, to debug all cores on a running application, without reflashing everything?
Thanks and regards,
Marcel Kummer.