This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: tcpEchoF2838X

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE, SYSBIOS

 tcpEchoF2838X.zip

I want to build the TI-RTOS, NDK, NS application form C2000Ware_3_04_00_00 and run it from flash. Within this application there is only the code for the CM. Without the right init form C2000 it can not run. Therefore I added my full project with separate code for the two processors. I the end I want to run the code from FLASH. The project from the C2000Ware_3_04_00_00 is buggy.

After installing ndk_f2838x_3_61_01_01 and ns_2_60_01_06 (Where I do find these both zip Files, I do not find it anymore at the Internet? I got the files from a collegue, who downloded them 1/2 year before). I could compile the project, but I got the following error: