Part Number: TMS320F280049C
Hi Champ,
I am asking for my customer.
May I confirm that the reserved field in GPIOB (GPIO 36 & 38) if it is written in 0 / 1 (access the pin), will it cause the MCU any problem ?
The customer prefers to access the GPIO32 ~ 39 as a byte at a time. Unfortunately, there are two reserved field in it.
They are facing a problem when debugging the code, it will stops at here.
As the TRM page. 869 Caution mentions it isn't allow to implement like this. Am I correct ?
Also, the customer would like to keep the same setting for the GPIOA and GPIOB in programming, access the GPIOs as a byte in one time.
They would not like to set GPIO32 ~ 39(except 36&38) one in a one time. Not only it keeps the code neat, also narrows down the code size.
Any suggestion to avoid of this or any ways for doing their wishing ?
Thanks for any help. Thanks !
BR, Johnny