This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C2802: TMS320C2812

Part Number: TMS320C2802


Hi,

I'm trying to install Code Composer version 3.1.23 on a brand new machine with Windows 10, 64bit, version 2H02 (build 19042.1237) and I first install the 3.1.19 version followed by the update to 3.1.23

I then try to install the driver for the board emulator I'm interested in (F2812PP) via a file called setupCCSPlatinum_v30118.exe  and when attempting to do that I get an error message as follows:

At the top of the error window I see: SD CCS 3.1 Emulation Drivers Error

The window contains message: Error 1925. You do not have sufficient privileges to complete this installation for all users on the machine. Log on as an administrator and then retry this installation.

I do have admin rights to the machine however. I also tried to install the drivers from the built-in admin account and I get the same error. I have installed this on multiple machines before without a problem (even on systems with a newer version of WIndows 10. Can anybody help with this please?

Thank you,

Ted