Other Parts Discussed in Thread: TMS320F28335
Hello All,
I have tried to send some data over the CAN interface of the C2000 f2806x but there is no activity on the TX and RX pins, pin 31 and 30, respectively. The pin voltages are always 3.3 V. Any idea why?
The code embedded on the C2000 is programmed in Simulink and it is composed of a eCAN transmitter block with a constant U32 integer as input.
The code for reading from the CAN bus is still in Simulink and it is composed of a CAN configuration block + CAN receive + CAN unpack.
The hardware setup is a f2806x control board mounted on a development board + CAN transceiver + PEAK-CAN USB receiver connected to a computer.
Please, any suggestion will be very welcome.
rgs
Francesco