This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: same memory location for two different variables in two different .cla file

Part Number: TMS320F28379D

Hi,

I am using F28379d processor. I am working with cla for an application. I have two .cla files in my code.

I notice that when a variable is declared in the second .cla file , it takes the first memory space of cla data memory which has already been used by some other variable in the first cla file:

for example:

File1 : clafile1 .cla

float32 x; 

Suppose this variable is stored in 0x9000.

File 2: clafile2.cla

float32 y;

This variable also gets stored in 0x9000.

How can i solve the above issue. it lead to errors in result. the memory location is getting modified by the other cla file.

Thanks,

Mukul